binding using template does not show count

Issue

When binding using templates at Release 1.1 the user is presented with the number of objects that were found, this count was missing in Release 1.2 and 1.3

Product Line

SmartStruxure Solution

Environment

Site with official release 1.2 and 1.3 versions

Cause

When binding using templates at Release 1.1 the user is presented with the number of objects that were found: 


 

 

this count was missing in Release 1.2:

Resolution

The Count feature will be available in upcoming release.