Issue
How can a 16 bit signed integer value be displayed correctly?
Environment
Modbus
IC
IC3
16 bit
Signed
Cause
A Modbus value is displayed as 65???.
Resolution
With a 16 bit signed integer value, the range used is +/- 32767, and seeing a value of 65??? indicates a negative value.
The easiest way to read this value is to use a lookup table.
The table should be added as follows.
0 = 0
32767 = 32767
32768 = - 32767
65535 = - 0