Issue
What are the part numbers for the IOU module terminals?
Environment
Netcontroller
Netcontroller II
IOU Modules (all)
Cause
Need to wire a remote or third party power supply to a Netcontroller; or to wire remote IOU modules. Not sure what parts need to be ordered for the module terminals.
Resolution
There are two separate terminals available, a male power supply connector and a female IOU module connector.
Male Power Supply Connector (Left Hand Side)
01-2050-285 (Male Connector for PS NetController)
Female IOU Module Connector (Right Hand Side)
01-0010-840 (IOU Module Connector, BOX OF 20)