Is it possible to save a copy of a TGML graphic in a standard format such as jpeg, bmp etc?

Issue

Is it possible to save a copy of a TGML graphic in a standard format such as jpeg, bmp etc?

Product Line

TAC Vista

Environment

TGML graphics editor 5.1.X

Cause

For documentation purposes a customer may wish to have an image of a TGML graphic, perhaps in a system reference guide, with explanatory text.

Resolution

  1. Open the graphic in TGML graphic editor.
  2. Select "Export..." from the file menu and then select the file format in the dialogue that appears.