Issue
Need to generate a list of all alarms in the system.
Environment
Vista
Cause
Vista has a search function to find out what alarm objects exist in the system.
Resolution
To search for all the alarm object in the system:
- In Workstation, click on Search
- Go to Type of devices and objects and click on the button right of view
- Search for "Event" and then "Message" mark "Alarm" and click ok
All objects are now listed and can be copied and pasted to an Excel sheet.