Issue
Is it possible to see a list of all the signals in the vista system that are overridden manually?
Environment
Vista 5.1.X
Cause
It is important for the customer to know which signals are manually overridden to be able to make appropriate decisions about a plants' status.
Resolution
There are 2 main options available:
1. Use Vista's search tool -the screen shot below shows which criteria to use. You can of course include other points in the filter.
2. Create a report and link to the signal's 'manual control' property. This option would have the advantage of being able to trigger the report via a button in TGML and that the layout can be configured according to the customer's specifications. However, it will take a bit longer to configure the report initially.
-Open the report and via the Vista reports addin configure a vista link to a value as shown below.