Where can I purchase a replacement battery for a MicroNet LCD (Low Cost Display)

Issue

Replacing battery

Product Line

Satchwell MicroNet

Environment

Panel
Wall mounted
Controller mounted

Cause

Old age

Resolution

RS Order number=         201-9438

Type LS14500

Click here to be linked to the RS page

Updated January 2014.
The MicroNet 50 series range MN350,450,550,650 LCD and Touchscreen have been withdrawn from sale.
Currently no direct replacement is offered.
The IAC 420, 600 and Touchscreen are not effected and remain available.