Issue
Can the ASD driver of the I/A Series UNC or ENC be connected to the ASD bus actively operating under a GCM?
Environment
I/A Series R2 and G3 ASD driver
Cause
Attempting to directly communicate to the ASD devices with two different systems simultaneously.
Resolution
The I/A Series UNC / ENC acts as the master of the ASD bus replacing the communications function of a GCM. Do not connect the GCM's ASD bus with the UNC / ENC's ASD bus. Connection of both devices to the same ASD bus will cause severe communications conflicts and improper bus operation.