Issue
Can Windows User be logged off when running ModBMS?
Environment
Satchwell ModBMS
Cause
There is a requirement for Windows User accounts to be logged off when not in use due to IT security concerns.
Resolution
A Windows User is required to be logged on when ModBMS is running. This is because the ModBMS application is not supported to run as a Windows Service. As such, ModBMS will stop running if the user logs out of Windows.