Sigma CE files are not created.

Issue

Sigma CE files are not created.

Product Line

Satchwell Sigma

Environment

Sigma CE 4.06

Sigma 4.06 

Cause

Sigma CE files are not created when BuildCE.exe is executed..

Resolution

A Sigma service pack is required.

Download here Sigma 4.06 SP1.

There is a readme.txt file for installation instructions included in the download.