Issue
How to determine if a Niagara G3 ENC or Jace is properly licensed for embedded Workbench.
This is an optional purchase (part # ENC-WB) and provides Workbench functionality through a web browser.
Environment
Niagara G3
Cause
Confirming that a purchased option is properly reflected in the license file (without actually trying out the feature).
Resolution
In the license file, the 'web' line will have the three variables set to 'true' in order to have embedded Workbench:
ui="true", ui.wb="true", ui.wb.admin="true"
If ui.wb.admin is set to "false", the station will be web-accessible but Workbench is not web-accessible.