Issue
Getting I/A Series G3 javax.baja.xml.XException error when attempting to configure proxy extension conversion as Generic Tabular.
Environment
I/A Series G3, ENC, JACE
Cause
The conversion selection Generic Tabular provides a way for a VoltageInputPoint or ResistiveInputPoint to support a non-linear responding signal on a universal input (using point Facets other than temperature). Generic Tabular uses a "lookup table" method similar to the "Thermistor Tabular" conversion, but without predefined output units. Selection provides a popup Tabular Conversion Dialog in which you can enter a custom source-to-result" non-linear curve, including the ability to import and export response curves. Use of Generic Tabular requires the kitIo module to be installed.
Resolution
Use the Platform Software Manager to install the kitIo module into the target ENC or JACE.