SmartStruxure Building Operation - Is there a way to force ES web clients to use https only (instead of http)?

Issue

Web Security.

Product Line

SmartStruxure Solution

Environment

http

https

Web Clients

Cause

http does not provide the same level of security as https.

Resolution

At SmartStruxure Building Operation 1.4, this is no way to force ES web clients to use https.

The feature is supported from SmartStruxure 1.6.0 RC and up