Issue
LON devices have the ability to run stand alone schedules. This capability requires continuous time updates.
Environment
Niagara G3
Cause
The LON Time object provides the ability to transmit the station's "System Time" to any LON device using an NVI SnvtTimeStamp type.
Resolution
The LON Time object provides the ability to transmit the station's "System Time" to any LON device using an NVI SnvtTimeStamp type.
- Install KitLon under Software Manager
- Open KitLon under Palette
- Drag or copy and paste the LonTime Object in the LonNetwork
- Link the LonTime Object time stamp to NVI Set Time