Out of range alarm does not work.

Issue

Out of range alarm attached to i2 device does not work when point's value is out of the range.

The 'Alarms' system variable in the controller shows 0

Product Line

Andover Continuum

Environment

CyberStation

All i2 devices

All InfinityControllers

Cause

Out of Range alarm is a BACnet alarm and can not be used with Infinity points

Resolution

Use Expression or Infinity Low/High Limit alarm type.