Set the Peripherals section of the Configuration Profile in I/NET Seven for Access Control

Issue

How should I set the Peripherals section of the Configuration Profile in I/NET Seven for Access Control? I am not using I/DISKs; and I do not have any access control hardware on these comm ports.

Product Line

TAC I/NET

Environment

I/NET Site

Cause

How should I set the Peripherals section of the Configuration Profile in I/NET Seven for Access Control? I am not using I/DISKs; and I do not have any access control hardware on these comm ports.

Resolution

Leave the ports at the default settings. Make sure you enable the Access Control option in the Workstation Options of the configuration profile.