Issue
Cyberstation Online Help for Workstation editor Time Tab contains incorrect information.
Environment
Cyberstation online help
Cause
The highlighted text in the Workstation Time Tab online help is inaccurate.
Note: When entering this number, use the opposite sign (negative or positive) from what you actually want the system to write. For example, if you are 300 minutes (5 hours) ahead of GMT, enter:
-300
For example, if you are -240 minutes (4 hours) behind GMT, enter:
240
Resolution
Under UTC Offset, the Note should read as follows:
Note: When entering this number, use an negative integer to specify time zones to the West (earlier than) Greenwich Mean time and a positive integer to specify time zones that are to the east of GMT.
For example, if you are 300 minutes (5 hours) ahead of GMT, enter:
-300
For example, if you are 240 minutes behind (later than) GMT, enter:
240