Does the JACE-6E or JACE-7 support multiple FTT-10A LON cards?

Issue

Does the JACE-6E or JACE-7 support multiple FTT-10A LON cards?

Product Line

TAC I/A Series

Environment

JACE-6E, JACE-7, LON FTT-10A

Cause

Application requires multiple FTT-10A LON trunks.

Resolution

Yes ... the JACE-6E / JACE-7can support two individual FTT-10A cards.  Purchase (2) TRD-NPB-LON (FT-10A Lon Adapter cards) and (1) ENC-DRV-LON driver.  Add one LonNetwork for each physical port.  Under each LonNetwork within the Lon Comm Config, specify the port's Device Name (e.g. LON1 and LON2).  Reference the Niagara AX Lonworks Guide for more details.