PE commands on b3 and i2 Controllers

Issue

Do all b3 and i2 Controllers support  all PE commands

Product Line

Andover Continuum, SmartStruxure Solution

Environment

b3 i2 Controllers String Trig

Cause

Some PE commands can not be used on some b3 or i2 controllers

Resolution

The following Plain English system functions are not supported in the i2885, i2885-V, and i2887(L) controllers: (b3885,b3885-V, and b3887(L) controllers:)

ACOS, ARCCOSINE, ARCSINE, ARCTANGENT, ARCTANGENT2, ASC, ASIN, ATAN, ATAN2, CEILING, CHR, CLOSELIST, COS, COSINE, EXP,
EXPONENTIAL, FACT, FACTORIAL, FIRST, FLOOR, GETOBJECT, LAST, LEFT, LEN, LENGTH, LN, LOG, MID, NUM_TO_STR, OPENLIST
RANDOM, RIGHT, RND, ROUND, SD, SEARCH, SIN, SINE, STANDARD_DEVIATION, STR_TO_DATE, STR_TO_NUM, STR_TO_TIME, STRINGFILL
TAB, TAN, TANGENT, VAL

See
- b3 technical data
- i2 technical data
- PE Programming guide