Viconics - How does the Occupation Sequence of a SE7200 controller operate.

Issue

How do the controller settings affect the Occupation Sequence in respect of temperature control.

Product Line

TAC Vista, Andover Continuum, Field Devices, SmartStruxure Solution, SmartStruxure Lite

Environment

Stand alone.

Part of a system.

Cause

Customer is uncertain of how this process works, the rooms are cold.

Resolution

There are a number of settings that will affect this sequence, the screen shot below shows the sequence and the settings used.