Issue
User over adjusts the setpoint on the STR612
Environment
STR612
Cause
The STR612 is used in conjunction with the CZU fan coil unit controller. The user over adjusts the setpoint.
Resolution
The STR612 setpoint dial can be restricted.
Under the dial cover are 2 plastic pegs that can be moved to the temperature extents that are required.