Issue
In Niagara G3, how many stations can connect to one Enterprise Network Server?
Environment
Niagara G3
Cause
Planning a large installation
Resolution
An Enterprise Network Server running on a 32-bit server can handle up to 150 stations.
An Enterprise Network Server running on a 64-bit server can handle up to 500 stations.