Is it possible to get a XIF from Lonmaker

Issue

Is it possible to get a XIF from Lonmaker when you have commissioned it by "upload" from device?

Product Line

TAC Vista

Environment

TAC Vista Toolpack

TAC Vista Server

LonMaker

Cause

If you don't have the XIF you can upload from the device in Lonmaker. There are no way to get this XIF out of lonmaker.

But TAC Vista system Plug-in will create a XIF for you when you import the device in TAC Vista.

Resolution

There are no way to get the XIF from Lonmaker but the system plug-in will create a new XIF when you add the device to the TAC Vista db.

Refer to article #6250 for a instructions on how to locate the XIF generated by the system plugin.