Issue
Error Message pop up reading:
Station Conflict - [Link: 95]
Station 00 at site 61 - Xenta527 conflicts with site 63 - xenta737-97.
Station Conflict - [Link: 1000]
Station 00 at site 03 - Host 3 conflicts with site 90 - Host 9.
Product Line
TAC INET
Environment
I/NET
Cause
Station conflicts occur when multiple devices share the same address. This is always the cause, but Identifying the possible addresses can be confusing.
- Host Address - The I/NET Configuration unique identifier for each host workstation. 1-250
- Link address - The system segment in question. Contains multiple Stations and in DLA multiple sites. 0-99 It is generally advised that you do not use Link 0. The Link will typically define an NPR or Xenta 527. Such as the Link 4 Xenta 527 functions as the bridge between TCP/IP and the Link 4 Controller LAN segment.
- Site Address - Only used in DLA architecture.(1-63) 0 is only used in non-DLA NPR devices. The site allows for multiple Controller LAN segments to use the same Link address. This changes the description of a Xenta 527-NPR from Link 6, to Link 6 Site 1 and allows Link 6 Site 2, Site 3 and so on. In DLA architecture, the NPR devices will typically all use the same Station Address. If link 6 Site 1 uses Station 0, Link 6 Site 2 may also use Station 0.
- Station Address - This is the unique identifier for addresses on a physical controller LAN wire. You may use 0-63, but one must be reserved for the NPR device. Station level controllers are typically referred to in messaging by a 4 digit address. Link 4 station 12 may be shorted to 0412. All controllers in an I/NET system must have a unique for digit label of LLSS. The only exception to this is the NPR device as it function as a gateway and can have a site address to make it unique. Controller LAN level controller do not show a site label.
Resolution
- Change the address on one of the offending controllers
- In DLA situations, you can only duplicate the Station address used by the Xenta 527
- If a 913 is used on the Controller LAN, it must also have a unique station ID
- Ensure all Host workstations have unique host ID's
- Ensure all devices in a DLA architecture have unique Link/Station combinations. There cannot be 2 Link 4 Station 3s, even if they both have a unique site number.