Issue
When ordering Veris products through Schneider Electric, SE part numbers must be used.
Environment
Veris products
Cause
Cross reference needed between Veris and Schneider Electric part numbers.
Resolution
Veris Part no | SE Part no |
H708 | 3240100000 |
H709HV | 3240101000 |
H308 | 3240102000 |
H608 | 3240103000 |
H908 | 3240104000 |
H909HV | 3240105000 |
H800 | 3240106000 |
H300 | 3240108000 |
H600 | 3240109000 |
H900 | 3240110000 |
H721LC | 3240201000 |
H721HC | 3240202000 |
H921 | 3240203000 |
H722LC | 3240204000 |
H722HC | 3240205000 |
H723LC | 3240206000 |
H723HC | 3240207000 |
H922 | 3240208000 |
H923 | 3240209000 |
H221 | 3240210000 |
H321 | 3240211000 |
AH01 | 3240301000 |
AH-27 | 3240302000 |