The Universal Input real-time values on a MNL-800 (or Microzone II) are fluctuating unrealistically.

Issue

The Universal Input real-time values on a MNL-800 (or Microzone II) are fluctuating unrealistically.  They rise, peak, drop, valley and then start over again very quickly.  It is similar to an AC wave pattern.

It is happening with all the inputs no matter their configuration.

Product Line

TAC I/A Series

Environment

MNL-800

Microzone II (Network 8000)

Cause

When an actuator is interfaced with a MNL-800 (or MicroZone II), and the UI cable shields are connected to earth ground (the SHLD terminal), the shield has a common mode AC potential that couples to the UI input. Only a very small signal (UI shield to signal common) is needed to result in objectionable UI signal fluctuation.

Resolution

Connect all drain shields on UI inputs to UI common (C terminal).

Read additional solutions and a more descriptive cause in Technical Bulletin 01-36.