Issue
Backup and Restore Process for StruxureWare Web Reports
Product Line
SmartStruxure Solution
Environment
SmartStruxure
WebReports
Reports Server
Cause
Need detailed backup process
Resolution
Backing Up the WebReports Database
- On the Windows toolbar, select Start, and then click SQL Server Management Studio.
-
Click Connect.
Note: When using a remote Computer to connect to the Report Server SQL database, the Windows Accounts must exists on both machines and have administrative rights for the SQL database otherwise a successful backup will not occur. In this instance it is recommended to use the SysAdmin 'sa' login / password details when connecting in remotely.
- Expand the Databases folder.
-
Right-click StruxureWareReportsDB, point to Tasks, then click Back Up.
-
Under Destination, click Add.
- Click OK.
-
In the Destination on disk box, select the backup destination.
- Click OK.
- Click OK.
Restoring the WebReports Database
- You restore the WebReports database to recover reports data from backup.
-
On the Windows toolbar, select Start, and then click SQL Server Management Studio.
- Click Connect.
-
Expand the Databases folder.
-
Right-click StruxureWareReportsDB and select Tasks, then select Restore, then select Database.
- In the Restore Database dialog box, select the database set(s) that you want to restore.
-
Click OK.
- Click OK.