A method to search Access Events for a specific Personnel during a specific period of time.

Issue

Want a method to show all the Access Events that a Personnel has had during a specific period of time.

Product Line

Andover Continuum

Environment

Continuum Access Control

Cause

A method to search Access Events for a specific Personnel during a specific period of time.

Resolution

One method to do this would be to use Listviews.

There are a number of default Listviews available in a default ContinuumDB and we can use one of these as a basis for our new Listview. See the dump file here where I copied the Events_Today Listview and added the prompt for a card number search using DBQualifier : (CardNumber is Prompt("Please Enter a Card number", 0) and Template = False)

This should return all the events today for the cardnumber that the user inputs in the prompt box when running the Listview.