Stem heater for V222/V292

Issue

Which stem heater should be used with V222 and V292?

Product Line

Field Devices

Environment

8800112000

8800113000

Cause

In some applications, a stem heater is required.

Resolution

For V222/V292, DN65-100, stem heater 8800112000 should be used.

For V222/V292, DN125-150, stem heater 8800113000 should be used.

For more information on stem heaters, see Lessons Learned Article #7856.