Issue
After upgrading the database from version 1.74 to 1.81 and converting the NC1 to NC2 all the doors produce the following error on reload.
Infinity controller error: Feature has not been enabled in this controller An error was detected while attempting to set an attribute in a remote Infinity object.
Environment
CyberStation
CX9680
ACX5720
ACX5740
Cause
New CardFormats2 column in the door table contains incorrect value.
Sending a door object from the database to a text file shows the following
InstanceId : 7001/7004
CardFormats : 4
CardFormats2 : 1246576928 <------------------------ this attribute should have an initial value of zero.
Description : DOOR 1.04
Resolution
Run the following SQL query to set the initial value of the new CardFormats2 column in the database to zero
update Door Set CardFormats2 = 0