STC contact temperature transmitter application

Issue

The STC series transmitter is delivered with a pipe clamp designed for maximum 100mm (4") pipe diameter. Is there any other solution if pipe diameter is larger than 100mm/4"?

Product Line

Field Devices

Environment

STC100

STC101

STC200

STC201

STC110

STC120

STC300

STC600

Cause

Included pipe clamp does not fit larger pipe size applications.

Resolution

If the application requires the transmitter to fit pipe with bigger outer diameter than 100mm/4", the included pipe clamp can be replaced with a bigger clamp purchased locally at the hardware store or similar.