Issue
If renaming a snippet in the graphic editor it will hang.
Environment
TAC Vista graphic editor 1.1.6
Cause
The problem is that a space is used in the end of the name, that will cause the graphic editor to hang
Resolution
Don't use space in the end of a snippet name or use an editor with version 1.1.7 or higher. This problem is corrected in version 1.1.7.