Issue
The ability to add a second card is available in webclient, but there is no where to add the second card
Environment
Windows XP
Windows Vista
Windows 7
Windows Server 2003
Windows Server 2008
Cause
Steps are needed to configure dual credentials to show in webclient, but those steps have not been completed.
Resolution
Steps to configure dual credential access in webclient: