Issue
Menta module names disappear when exporting a Xenta from Vista version 5.1.8 and importing it to Vista version 5.1.7
Environment
TAC Vista 5.1.7 and 5.1.8
Cause
Changes is made in the export/import function in TAC Vista 5.1.8 which will cause problems to import a export file from TAC Vista 5.1.8 in to TAC Vista 5.1.7.
Resolution
To be sure that the export/import function should work only export and import between Vista systems of the same version.