Can a DPU be added to an existing 7792 SubLAN?

Issue

Can I add a DPU on an existing 7792 Sublan?

Product Line

TAC I/NET

Environment

  • 7910 DPU
  • 7920 DPU
  • 7792 SubLAN

Cause

The 7792 are for MRs and ASCs only.

Resolution

A DPU cannot be added on an existing 7792 Sublan. 

To correct this:

  1. Do a Memory Clear on the controller with a HHC.
  2. With the HHC, change the controller to a 7793.
  3. This will allow you to have MRs, ASCs And DPUs on the same SubLAN.