Changing the panel layout

Issue

The initialization of a panel does not adjust the size of objects in the panel. Once a panel is created, how to re-adjust each object's size in it?

Product Line

SmartStruxure Solution

Environment

SmartStruxure version 1.3

Cause

When creating a panel in the WorkStation, the system does not have a step asking to adjust the size of each object (graphic, trend chat, etc.) in this panel. Users need to do additional setting in the WorkStation in order to change the layout.

Resolution

  1. Create a panel according to the customer's demand.
  2. Right click on the panel just created, and select edit panel.
  3. In the right side panel, adjust the panel layout.
  4. Once the change is finished, click on the Save button on the top of the tab.

Reopening the panel will find the panel now is planned as desired.