Will there be an app for Android / iOS to control Vista

Issue

  • Need an Android application for Vista
  • Need an iOS application for Vista
  • Need an iPhone application for Vista
  • Need an Tablet application for Vista

Product Line

TAC Vista

Environment

  • mobile
  • tablet

Cause

Some people have asked for an application to control Vista via Android phones or iPhones and tablets.

Resolution

There will probably not be an application for mobiles or tablets for the Vista environment.
There are plans in work on implementing web services in to Vista. This means that with the help of a StruxureWare Building Operation frontend you can use the StruxureWare Building Operation application for tablets and phones to work with Vista.