Can Continuum CyberStation run on Windows 8?

Issue

Most PCs are now shipping with Windows 8 and many drivers for Windows 7 do not exist for the hardware.  

Product Line

Andover Continuum

Environment

Windows 8, CyberStation

Cause

New PCs and laptop are shipping with Windows 8 and Windows 7 drivers are not available for some newer hardware.  

Resolution

At this time CyberStation 1.94 and 2.0 are the versions that are shipping and no versions of Windows 8 have been tested with CyberStation.

It has not been determined whether a future version of CyberStation will be qualified on Window 8.

Refer to the Software and Firmware Compatibility Matrix for the operating systems compatible with CyberStation.