StruxureWare Building Operation 1.3.0 SP1 Installation

Issue

Problems after installation of Service Pack 1

Product Line

SmartStruxure Solution

Environment

SmartStruxure 1.3.0 SP1 Build 10100

Cause

The Service Pack must be installed on top of an existing 1.3.0.938 build of Building Operation

Resolution

To use the Service Pack:

  1. Install or verify installation of 1.3.0.938
  2. Run the installers (see link below if you require additional detail)
  3. Be sure to select the "Upgrade" and not the "Uninstall" option 

The Online help (link below) provides a step by step workflow for this Service Pack, so you require additional detail.

http://help.sbo.schneider-electric.com/Topics/show.castle?id=9389&locale=en-US&productversion=1.3&a=1