Which models of the SE7300 series room controllers can be used with the SC3000 series relay packs?

Issue

Which models of the SE7300 series room controllers can be used with the SC3000 series relay packs?

Product Line

Field Devices, SmartStruxure Solution, SmartStruxure Lite

Environment

SE7300 series Room Controllers

Cause

The SC3000 series relay packs allows existing line voltage wiring between the fan coil unit and temperature controller to be re-used. Only certain models of the SE7000 series room controllers can be used with the relay packs. 

Resolution

The SER7300 is used with the SC3000.
Refer to F-27797 SER7300 and SC3000 Series datasheet. Refer to the F-27777 SC3000 Series datasheet to select the appropriate relay pack for your application. 

SE7000 series Room Controllers documentation can be found on The Exchange Download Center.