Too Many Panels dialog box when opening 9th panel in Pinpoint

Issue

A dialog box pops up in Pinpoint "Too many panels opened. Please close some to continue." when attempting to open 9 panels

Product Line

Andover Continuum

Environment

Continuum

Pinpoint

Windows XP

Windows 7

Windows Server 2003

Windows Server 2008

Cause

A limitation has been built into 1.94 to restrict the number of panels because having that many panels open can cause instability with the Pinpoint application.

This is a hard coded restriction in the code.

Resolution

There can only be 8 panels open in Pinpoint. Add points to another panel, but keep an eye on performance.

Ultimately there should be less 100 links per panel

http://buildingskb.schneider-electric.com/view.php?AID=11478