Supported LoyTec L-IP Operating Modes in StruxureWare for Building Operation

Issue

What mode does a LoyTec L-IP need to be configured in to work with StruxureWare for Building Operation?

Product Line

SmartStruxure Solution

Environment

Loytec L-IP

Enterprise Server

Cause

The operating mode limits the capabilities of the LoyTec L-IP when used with an Enterprise Server

Resolution

Ensure that the LoyTec L-IP is in Smart Switch mode.

This is achieved by using the DIP switch settings for switch 1 and 2 in the ON position.

 

For additional detail please reference the LoyTec L-IP user manual.