Issue
For EpiDesigner or EpiBuilder to work with some devices a plug-in needs to be purchased.
Product Line
Andover Continuum
Environment
Continuum
EpiBuilder
EpiDesigner
Windows XP
Windows 7
Windows Server 2003
Windows Server 2008
Cause
Epibuilder will not communicate with some approved devices without purchasing a special plug-in.
Resolution
ImageWare is the third party company that Continuum integrates with for badging and there are a number of devices that require a plug-in to work.
Check the following web page for a list of tested and supported items and if the device indicates plug-in, then purchasing a plug-in is required.
http://support.iwsinc.com/Support/EPISuite_compatible_hardware.cfm
The plug-in can be purchased through a ImageWare partner.
http://www.iwsinc.com/partners/channel-partners
Schneider Electric does not sell the plug-ins and has no access to any serial numbers that may be prompted for during the installation.