Issue
Can Personnel be deleted or disabled in Continuum utilizing the PIU and a third party system?
Environment
Continuum
Personnel Import Utility
LDAP
Cause
Not sure what can be accomplished with the PIU to manage Personnel changes.
Resolution
The Personnel Import Utility, with the help of a transformation file, can be used to disable Personnel records in Continuum. This can be accomplished with an interface using LDAP, CSV, or XML.
One method would be to use the expiry date field to disable Personnel Access.