Dimensions for the back plate used with the ENCL-300-TUB.

Issue

Dimensions for the back plate (part # ENCL-300-BKP) used with the ENCL-300-TUB.

Product Line

TAC I/A Series, Field Devices

Environment

General Hardware

Cause

Dimensions not listed in iPortal

Resolution

Length = 28"     Width = 22.5"     Depth (thickness) = 0.5"