How to setup a BACnet MSTP Schneider Electric heat meter

Issue

What configuration is required for a Multical BACnet heat meter

Product Line

Andover Continuum, Field Devices, SmartStruxure Solution

Environment

Schneider Electric (Kamstrup) heat meter connected to a Continuum or SmartStruxure system on MS/TP.

Multical 61/62/601/602/801

Cause

Setup information required

Resolution

With the BACnet interface card fitted in the Multical meter it is a native BACnet MS/TP device.

Connect it to the AS or bCX1 depending on your system and Learn/ find BACnet devices. It should appear online and allow the objects to be uploaded.

A typical unit like the Multical 602 will contain 12 Analog Inputs for all of the information from the meter.

The Meter will operate at 9600, 19200, 38400, 57600 and 76800 Baud rates and autobaud to the connected system.

For the Datasheet  Click Here.

For the BACnet PICs statement Click Here.

Further information on the heat meter range is available on the Extranet: http://buildings.schneider-electric.com/Navigate?node=9994