Can a copy of WorkPlace Tech installed in a pc with Windows 7 virtual XP mode be copied to other Windows 7 computers and work?

Issue

An owner customer has purchased a non-expiring copy of WorkPlace Tech.  It is installed on a 64-bit Windows 7 computer within the XP 'mode' virtual machine.  Can it be copied to other Windows 7 computers and work or does the WorkPlace Tech license prevent it from working?

Product Line

TAC I/A Series

Environment

Windows 7

WorkPlace Tech 5

Cause

Loss of potential sales

Resolution

WorkPlace Tech licensing is not designed to identify a virtual 'hard drive' from an actual hard drive.  As a result, an installed copy of WorkPlace Tech will work in the virtual machine no matter how many Windows 7 computers into which it is installed.