What is the Part Number for the optional battery for the JACE-NXT (TRD-NXT-R2)?

Issue

What is the Part Number for the optional battery for the JACE-NXT (TRD-NXT-R2)?

Product Line

TAC I/A Series

Environment

I/A Series R2, JACE-NXT (TRD-NXT-R2)

Cause

An optional battery is required for the JACE-NXT (TRD-NXT-R2).

Resolution

The part number for the optional battery is TRD-NPB-BATT, per the Spec Data sheet for the JACE-NXT, F-27769.

There is also an optional UPS that includes a battery, TRD-NXT-UPS, per Lessons Learned Article #7754.

See Product Announcement PA-00223 for further information on the JACE-NXT.