Field Devices - What is the replacement for an AF24-S damper actuator?

Issue

Replacement an AF24-S Actuator?

Product Line

Field Devices

Environment

AF24-S

Damper

Cause

Customer requires a replacement actuator for a AF24-S.

Resolution

The AF24-S is a 24v power open, spring return damper actuator, it has a torque of 15 Newtons. To view the data sheet, please click HERE.

The replacement actuator range is the MD10SR/MD20SR ranges.

The MD10SR damper actuators have a torque of 10 Newtons (dampers up to 2m2) and are available in the models shown below. To view the full data sheet, please click HERE.

 

The MD20SR damper actuators have a torque of 20 Newtons (dampers up to 4m2) and are available in the models shown below. To view the full data sheet, please click HERE.

In the specific case of the AF24-S the replacement would be the MD20SR-T or -TS if auxiliary switches are required.