Issue
Niagara R2 hosts in a Microsoft Windows Server Environment
Environment
Niagara R2
Cause
Replacing a UNC-6x0 with a UNC-520 reduces the feature set available when connected to a Windows network.
Resolution
Summary table listing the features of Niagara R2 hosts on a Windows network. A JACE-NP is a UNC-6x0. A JACE-5 is a UNC-520. A JACE-4 is a UNC-410.
This table can also be found in the Network Connectivity Guide, Chapter 3, Table 3-1, page 3-5.